MODBUS.EN

Description

Enables or disables the Modbus interface.

0 = Disabled. All Modbus messages are ignored.
1 = Enabled (default). Modbus messages are managed by the drive.

Example

The following stops any Modbus messages from being processed.

-->MODBUS.EN 0
-->

Context

For more information, see Modbus Installation and Setup.

Versions

Action Version Notes

Implemented

02-05-00-000

 

General Information

Type

Read Write Parameter

Units

N/A

Range

0 or 1

Default Value

1

Data Type

Integer

See Also MODBUS.INFO

Stored in Non-Volatile Memory

Yes

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

MODBUS.EN

3014h

01h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

MODBUS.EN

3702

E76

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

MODBUS.EN

3702

Unsigned8

Read/Write

-